Unable to generate code for SE051C2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to generate code for SE051C2

368 Views
yashbawankar
Junior Contributor I

Hello Team, I am trying to Integrate SE051 with FRDM-MCXN947 board, by reading AN13030 guide, I followed all the steps till running python script to generate code but I am getting this error: 

Could not find 'cmake.exe'. Assuming 'cmake.exe' is in path and running.
INFO:__main__:Preprocessing C:\Users\yash.bawankar\Downloads\se05x_mw_v04.08.01\simw-top/ext/open62541/tools/schema/Opc.Ua.NodeSet2.Minimal.xml
INFO:__main__:Generating Code for Backend: open62541
INFO:__main__:NodeSet generation code successfully printed

Please let me know what am I missing.

0 Kudos
Reply
1 Reply

323 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @yashbawankar ,

 

Are you building the MW under windows? If yes, please make sure the following Prerequisite are met:
• Visual studio installed
• Python 3.8 32 bit installed
and please refer https://www.nxp.com/docs/en/application-note/AN12398.pdf  for more details on prerequisite installation steps. and you may find cmake install steps in chapter 8 within https://www.nxp.com/docs/en/application-note/AN12398.pdf .

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply