USDHC Support in MCXN947

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USDHC Support in MCXN947

2,482 次查看
JoseTepetla
Contributor II

Hi,

I'm trying to use the USDHC periphepal in the MCXN947VNL microcontroller, but the Pin Config tools displays errors when I change the package from MCXN947VDL (184 pins) to MCXN947VNL (100 pins). Do you know if there is support for this periphepal in ConfigsTool? 

  • Also I tried running an example from the SDK in a FRDM-MCXN947, but it works fine on that board. The problem just shows when I switch the uC package

I tried with the latest sdk (v2.16.100 and 2.16.0) but it always shows the same error. Also I'm using MCUXpresso v11.10.0 - MacOs

If there is not support for this, can you please share if there is a guide to setup the peripheral?

JoseTepetla_0-1727909750322.png

FRDM-MCXN947 

 

标签 (1)
标记 (1)
0 项奖励
回复
5 回复数

2,423 次查看
JoseTepetla
Contributor II

Hi Hang,

Can you share me which versions of MCUXpresso and MCXN SDK are you using in your setup?

Actually I'm using this ones (SDK 2.16.100-MCXNxx and the SDK of the FRDM board) 

JoseTepetla_0-1728483701478.png

 

0 项奖励
回复

2,379 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @JoseTepetla 

My SDK version is also SDK 2.16.100-MCXNxx,

And my versions of MCUXpresso is MCUXpresso IDE v11.9.1_2170.

BR

Hang

0 项奖励
回复

2,429 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @JoseTepetla 

I try to reproduce this issue.

HangZhang_0-1728465253451.pngHangZhang_1-1728465274950.png

But when i change the package from MCXN947VNL (100 pins) to  MCXN947VDL (184 pins).

It did not report how the error occurred.

BR

Hang

0 项奖励
回复

2,416 次查看
JoseTepetla
Contributor II

@Harry_Zhang 

I installed both versions of MCUConfigsTools (v15.1 and v16.1), in the latest one I can't find the USDHC peripheral. Do you know if there will not be more support for the latest version of the tools? 

Screenshot 2024-10-09 at 8.51.28 a.m..png

标记 (2)
0 项奖励
回复

2,375 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @JoseTepetla 

If i use MCUXpresso ConfigsTools v16.1,  I also can't find the USDHC peripheral.

I will report this issue to the MCUXpresso ConfigsTools IDE team.

Thanks for your information.

BR

Hang

0 项奖励
回复