Supported eMMC version in MCUXpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Supported eMMC version in MCUXpresso

1,223 Views
ljs1004
Contributor I

Hi, all

I'm trying to boot from eMMC, and also make the image using MCUXpresso.

I have a query about it, which version can be supported in tool & driver?

I found the lastest version for eMMC(v5.1B) which is released last year.

It's working with new version properly as well?

Labels (1)
0 Kudos
Reply
2 Replies

1,155 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @ljs1004,

Thank you for contacting NXP Support!


Please note that the i.MX93 is not an MCU, but rather an applications processor.


According to the datasheet, the supported eMMC standard is eMMC 5.1. I am not fully certain about the specific differences between versions 5.1 and 5.1b, but to ensure compatibility and avoid unexpected issues, I recommend using devices that comply strictly with eMMC 5.1.


Best regards,
Chavira

 

0 Kudos
Reply

1,094 Views
ljs1004
Contributor I

Thank you for reply.

I'm having some trouble which is not booting up properly.

Thus I'd like to know that there is any sequence to check eMMC version in MCUXpresso.

Especially there is change in v5.1B : 

EXT_CSD[192] : 0x8 -> 0x9

 

 

0 Kudos
Reply