Request for Hall Sensor-Based Motor Control Reference Firmware and Training Material

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Request for Hall Sensor-Based Motor Control Reference Firmware and Training Material

130 Views
Darshan_J_L
Contributor I

Dear NXP Team,

We are working with a customer developing an air-cooling system using a 24 V, 3.47 A motor.

We have successfully completed a demonstration using sensorless FOC-based motor control. The customer now wants to integrate Hall sensors for rotor position detection using the FRDM-MCXA156 EVK (control card) with the FRDM-MC-LVPMSM (power card).

Could you please suggest a suitable reference firmware or application example for implementing Hall sensor-based motor control on this hardware combination?

I reviewed the Hall-sensored BLDC example for the LPC55S36 available on GitHub.

However, I could not locate the corresponding FreeMASTER configuration file (.pmpx) for this example.

Could you please help us with the following?

  • Reference firmware for Hall sensor integration on the FRDM-MCXA156 with the FRDM-MC-LVPMSM.

  • The corresponding FreeMASTER project/configuration file (.pmpx), if available.

  • Relevant application notes, training materials, or implementation guides for integrating Hall sensor feedback into an existing sensorless FOC project Based on FRDM-MCXA156 EVK.

Your technical guidance and recommendations would be greatly appreciated.

Best Regards 

Darshan J L 

WPG India 

0 Kudos
Reply
1 Reply

105 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @Darshan_J_L ,

Thanks for your post.

The MCUXpresso SDK includes multiple motor control example projects. You can find more information for FRDM-MCXA156 on the following page.
 
The pmsm_enc example for the FRDM-MCXA156 + FRDM-MC-LVPMSM combination is in the SDK v25.06. It supports sensorless and sensored FOC and includes the pmsm_float_enc.pmpx FreeMASTER project. You can refer to UG10247.pdf for more details.
 
About the corresponding FreeMASTER configuration file (.pmpx) for LPC55S36 demo, you can find it here: an-lpc55s36_mc_bldc_whall/LPC5536_mc_bldc_wHall.pmpx at main · nxp-appcodehub/an-lpc55s36_mc_bldc_wh...
 
Hope it helps. Please let me know if you still have any other questions.
 
BR
Celeste
 
 

0 Kudos
Reply