Operations over the SD card on MCX A14x/A15x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Operations over the SD card on MCX A14x/A15x

1,071 Views
Doly02
Contributor I

Hello I would like to use MCXN EVK For Data Logging Application with this shield: https://botland.store/arduino-shield-communication/8238-datalogger-shield-v10-rtc-ds1307-with-sd-car..., is unfortunately I didn't find any example for writing/reading from SD card that I could use. Is there an example to base it on?

0 Kudos
Reply
1 Reply

1,030 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Doly02 

You can download the SDK_2_14_0_FRDM-MCXN947 from the NXP official websit.

Under this path SDK_2_14_0_FRDM-MCXN947\boards\frdmmcxn947\sdmmc_examples

You can find the SD example.

Hope this will help you.

BR

Hang

0 Kudos
Reply