Operation together between Pretended Networking mode and Doze mode (or Stop mode) - FlexCAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Operation together between Pretended Networking mode and Doze mode (or Stop mode) - FlexCAN

1,454件の閲覧回数
Phu_Le
Contributor I

In Pretend Networking mode, the CHI clock is turned off, keeping only the PE clock active to capture messages that match the filter. Meanwhile, in Doze mode or Stop mode, FlexCAN requires all clocks of both CHI and PE to be turned off. However, according to the Reference Manual, the PN mode can operate together with Doze mode or Stop mode. I want to understand how this is possible.

Phu_Le_0-1747896234306.png

 

0 件の賞賛
返信
3 返答(返信)

1,419件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Phu_Le 

May I ask which chip you are using?

BR

Harry

0 件の賞賛
返信

1,415件の閲覧回数
Phu_Le
Contributor I
Thanks for reply. I'm using MCX W71 MCU
0 件の賞賛
返信

1,360件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi

In MCX W71 Reference Manual

52.3.1.1.5
Pretended Networking (PN) mode
This special low-power mode receives wake-up messages with low power consumption. This mode can be selected to operate together with Doze mode or Stop mode. Before entering a low-power mode, MCR[PNET_EN] must be 1. 

This means:

PN mode is specifically designed to work in conjunction with MCU low-power modes.

While in Doze or Stop mode, CHI (Protocol engine) clock is shut down, but CAN_PE (Physical Layer Engine) remains active to monitor the CAN bus and detect wake-up events.

BR

Harry

0 件の賞賛
返信