Hello,
We are migrating from an MX8X controller to MX8MP. In the older one, ENET0 and ENET1 supported voltage 1.8V, 2.5V, 3.3V (RMII all three, RGMII first two only).
MX8MP removes the 2.5V option, but allows 1.8V and 3.3V choices. Absolute Vmax is 3.8V. The question is, what happens in a 2.5V operation on NVCC_ENET? 2.5 will not exceed the absolute max. But how are the MAC signals configured and what kind of impact would 2.5V operation have long term?
I ask because it would be great to avoid updating the older PHY that is currently running both its supply and VDDIO on 2.5V.
Thank you,
Mike