MCXE31B Firmware Flashing Using SPI Without Debug Probe

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCXE31B Firmware Flashing Using SPI Without Debug Probe

2,864 Views
blessyvinolin
Contributor II

Since MCX E31x devices do not support ISP mode and boot only from internal flash, is it possible to implement a custom SPI-based bootloader to enable firmware updates without using a debug probe? If yes, what are the required memory regions and boot configuration considerations?

Tags (1)
0 Kudos
Reply
7 Replies

2,839 Views
marek-trmac
NXP Employee
NXP Employee

Hi @blessyvinolin 

ISP mode for MCXE31x is supported via flashloader application, which supports UART and SPI. The flashloader is by default present in flash and started in boot.

See details here: Processor-specific workflows — Secure Provisioning Tool 25.12

 

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button

2,817 Views
blessyvinolin
Contributor II

Hi marek,

I am working with the MCXE31B and using the MCUXpresso Secure Provisioning Tool for flashing.

Current Setup:

  • flashloader.bin is first programmed into the device using a debug probe.
  • I have connected a USB-to-TTL converter to LPUART0.
  • After the flashloader is programmed, then the tool flash my application binary (led_blinky.bin) through UART.

Issue:

Whenever I power off or reset the board, the flashloader is no longer available, and I must again use the debug probe to flash flashloader.bin before I can program the application.

 

Is it possible to flash the application only using UART, without using the debug probe every time?

Can the internal ROM bootloader of MCXE31B be used for UART flashing?

What boot configuration is required to enable UART-only flashing?

Any guidance would be appreciated.

Thanks.

 

Regards,

Blessy

0 Kudos
Reply

2,805 Views
marek-trmac
NXP Employee
NXP Employee

Hi @blessyvinolin 

> Can the internal ROM bootloader of MCXE31B be used for UART flashing? What boot configuration is required to enable UART-only flashing?

There is no bootloader in ROM of this device. The UART ISP (ISP = In System Programming mode) is supported via flashloader only. 

 

> Is it possible to flash the application only using UART, without using the debug probe every time?

You can use another bootloader instead of the flashloader, that supports such feature. See for example MCUboot | mcuboot

 

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button

2,649 Views
blessyvinolin
Contributor II

How can I flash the image only using uart without using debug probe?

0 Kudos
Reply

2,645 Views
marek-trmac
NXP Employee
NXP Employee

Hi @blessyvinolin 

> How can I flash the image only using uart without using debug probe?

Chips where debug probe is not needed: Processor-specific workflows — Secure Provisioning Tool 25.12

And chips where debug probe is needed: Processor-specific workflows — Secure Provisioning Tool 25.12

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 Kudos
Reply

2,641 Views
blessyvinolin
Contributor II

Hi Marek,

Currently, I am facing the following issue:

Whenever I power off or reset the board, I need to connect the debug probe to flash the flashloader first. After that, I am able to flash my application image using UART.

However, my requirement is:

I want to flash the MCXE31B directly using UART without connecting the debug probe every time after power-on or reset.

 

Regards, 

Blessy

0 Kudos
Reply

2,638 Views
marek-trmac
NXP Employee
NXP Employee

Hi @blessyvinolin 

once the chip is not in factory state, SEC tool does not support provisioning without debug probe. 

You can implement your own application updates in your custom application, that was provisioned first time into empty processor.

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 Kudos
Reply