MCXA153 SystemCoreClock default value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCXA153 SystemCoreClock default value

1,498 Views
HugoArends
Contributor I

Intro

After a reset, he MCXA153 microcontroller runs ate 48MHz, because:

  • After reset, SCS bits in SCG->CSR = [011] : FIRC
  • After reset, FIRC (fro_hf) = 48 MHz, as stated in Reference Manual paragraph 21.2 (Rev. 7, 2024-10-22)
  • After reset, DIV bits in AHBCLKDIV = [00000000] : prescaler = 1

Problem

In the MCUXpresso SDK (26_03_00_pvw1), the SystemCoreClock global variable is configured in the function SystemCoreClockUpdate() in the file system_MCXA153.c. This is correct if the fsl_clock driver is used. If this driver is not used, the SystemCoreClock variable is set to 12MHz, which is not correct.

As a suggestion, update the following

In the file system_MCXA153.h, update the define:

#define DEFAULT_SYSTEM_CLOCK           12000000u           /* Default System clock value */
#define DEFAULT_SYSTEM_CLOCK           48000000u           /* Default System clock value */
 

In the file system_MCXA153.c, update the function SystemCoreClockUpdate() so it does not depend on the fsl_clock driver anymore and uses direct register access.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,456 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @HugoArends 

 

Thanks for your suggestion. I will report it to your internal team.
Thank you.
 
BR
Alice
0 Kudos
Reply