MCX A secure/signed mode in rom bootloader?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCX A secure/signed mode in rom bootloader?

1,263 Views
dav1
Contributor V

Lets assume we want to design a system using MCX A-series that uses the ROM bootloader feature for end-customer firmware upgrades. 

Upgrades could happen via web-serial->usb or in-system updates via UART from another mcu, both talking directly to the rom boot code. 

I haven't looked in detail whats available in the newer MCX-series rom implementation, but the questions are:

  • is there a way to require a signed binary when using ROM boot?
    • i.e. write "otp-keys" to flash and force the bootloader to only accept valid binaries to be written

  • are there ways to prevent raw reads from flash while still having erase/write enabled?

 

in my case mcu pick would be: MCXA156VPJ

 

 

ps. fully aware I can write my own 2nd stage BL to achieve this, but the whole point here is to design a simple + brick-proof system.

0 Kudos
Reply
2 Replies

1,232 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @dav1 

The MCXA series does not support secure or signed mode in the ROM bootloader.
Please consider using the MCXN series, which does support this feature.

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc... 

Thank you.

BR

Alice

0 Kudos
Reply

1,098 Views
dav1
Contributor V

1)

the N-series are too expensive for the application.
what other mcx'es do support secure rom-boot?

 

2)

are you 100% sure there isn't a way to achieve a secure update-path on A-series?

0 Kudos
Reply