I2c communication not happening (slave side)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I2c communication not happening (slave side)

1,352 次查看
Ramanju_BV
Contributor I

I tried the  FRDM -MCXN947 master slave I2C example  and setup the  jumper settings J2_20 , J2_18 ,J2_14 from the  both end  ,it is working  fine  .

For my requirement I need to change the salve pin configuration to j9_32 , j9_30 and j9_24 pins .and  accordingly i configured the  slave pins too .

But I'm not able to transfer the data . Showing  NACK in master .
Do i need to change any configuration ? 
Could you please someone help me  with that . ?
Thanks  in advance .

0 项奖励
回复
2 回复数

1,209 次查看
Ramanju_BV
Contributor I

Sure. Thankyou for the reply .

0 项奖励
回复

1,302 次查看
Joey_z
NXP Employee
NXP Employee

Hi,Ramanju_BV

Sorry for the late reply.

P1_8,P1_9 is not an I2C peripheral pin, please change to another I2C pin.

XuZhang_0-1727167941914.png

XuZhang_1-1727168117858.png

 

BR

Xu Zhang

 

0 项奖励
回复