How to understand IO structure diagram

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to understand IO structure diagram

1,646 Views
SiLongWu
Contributor I

How to understand General purpose IO structure diagram and pad control register?

Here are relative pictures below. 

Why does ODE take the opposite, then perform "&" operations with Pull_Keeper_Enable, and then take the opposite of the computed result? In the description of register, Pull_Keeper_enable when Pull_Keeper_Enable == 1. So the diagram are different from the description of register.

What is the meaning of pull_en_b?

Why is there no Pull_Enable to work in the diagram?

In input mode, why are two inverters connected in series, and how can they take effect? Is their function to latch input data or to act as a delay circuit?

gpio_pad_structure.png_pad_ctl_pad_.jpg

Labels (1)
0 Kudos
Reply
1 Reply

1,570 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @SiLongWu 

 

Could you please tell me which chip you are using?

 

BR

Alice

 

 

0 Kudos
Reply