FRDM-MCXW72

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-MCXW72

1,028 Views
brianmohlman
Contributor III

Hello,

I just received two FRDM-MCXW72 boards, I have MCUXpresso for VCS setup and was going to try to compile/run the wireless ranging example. I saw a note that the NBU should be updated to the latest, but in the binaries folder I do not see a file for the FRDM-MCXW72 with HADM in the file name there are only two. and they are:

mcxw72_nbu_ble_all_hosted.bin

mcxw72_nbu_ble_xp_hosted.bin

Does either of these include HADM in them? 

Also, when will training materials be available, and when will the FRDM-MCXW72 board be a selection in the SDK builder tool 

Labels (3)
0 Kudos
Reply
1 Reply

955 Views
sofiaurueta
NXP Employee
NXP Employee

Hello, hope you are doing well.

 

To run the wireless ranging examples in MCXW72, the "mcxw72_nbu_ble_all_hosted.bin" file can be used, as this binary file includes supported HADM/CS features. The FRDM-MCXW72 SDK can be downloaded from the MCUXpresso SDK Builder and the binary files are provided in the following SDK path: ../mcuxsdk/middleware/wireless/ble_controller/bin

 

You can also follow this guide: Wireless ranging demo application setup — MCUXpresso SDK Documentation

 

Hope this helps!

 

Best regards,
Ana Sofia.

0 Kudos
Reply