FRDM-MCXA947 BLCD demo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-MCXA947 BLCD demo

1,751件の閲覧回数
CarlLee
Contributor III

Dear all,

I follow an App note AN14258 for Sensorless BLDC motor control on MCXA153 board and get the demo code from https://github.com/nxp-appcodehub/an-mc-bldc-mcxa153. After build and download to FRDM-MCXN947 board, it run properly when I press the key SW2 to start and stop the motor.

BUT when I follow the App note AN14258 page 13 (point 11) to test the code with FreeMASTER, the file bldc_frac.pmpx cannot be found in the code package.

Please Advice,

Thanks,

Regards,

Carl

ラベル(2)
0 件の賞賛
返信
1 返信

1,722件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @CarlLee 

Sorry this freeMaster file can not be upload for some limitation. 

There are two methods. The one method is to use SW2 button. The another method is to download SDK_2.9.0_FRDM-KE15Z. There is a freeMaster file under SDK_2.9.0_FRDM-KE15Z\middleware\motor_control\freemaster\bldc.pmp.  Change the .map file.  

 

BR

Alice

0 件の賞賛
返信