Ecc or External to internal clock auto-switch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ecc or External to internal clock auto-switch

947 次查看
Crshi
Contributor II

Hi,

 I'm here again with more curiosity.

I wonder that is following mechanisms available in k26 or mcxn mcu series:

1. Memory Ecc,

2. External oscillator stability  detecting

3. Auto switch from External clock to inner clock when external clock is abnormal

Nothing is mentioned in rm about the three aspects.

Looking forward for your reply. Thx

 

标签 (3)
标记 (4)
0 项奖励
回复
1 回复

881 次查看
Pablo_Ramos
NXP Employee
NXP Employee

Hi @Crshi,

The MCXN features up to 512 KB of RAM, which can be configured as up to 416 KB with ECC (supporting single-bit correction and double-bit detection). For more details, refer to Chapter 30, Error Recording Module (ERM), in the Reference Manual.

Additionally, it includes the SCG module, which contains a clock monitor capable of detecting the loss of an external clock (when enabled) and identifying changes in clock frequency. See Section 34.3.3, SCG LOC Operation, for more information.

The Kinetis K26 includes the Multipurpose Clock Generator (MCG) module, which features an external clock monitor with reset and interrupt request capabilities. This allows detection of external clock failure when operating in FBE, PEE, BLPE, or FEE modes. Refer to Chapter 27, Multipurpose Clock Generator (MCG), for further details.

Best Regards,

Pablo

0 项奖励
回复