Do the MCXA153 drivers support I3C HDR-DDR mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do the MCXA153 drivers support I3C HDR-DDR mode?

779 Views
ASM
Contributor I

Hi,

  In the example code I have, I can see that there is at least some code to support DDR, but it doesn't seem to work. Is it fully implemented, and if so, is there an example of how to use it?

  Thanks

0 Kudos
Reply
1 Reply

764 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @ASM,

As mentioned on the following community post: Solved: Re: Does RT685 support I3C HDR-DDR mode? - NXP Community

HDR-DDR mode has issues on both the RT and MCX A devices, so please use SDR instead.

BR,
Edwin.

0 Kudos
Reply