Config Tool for MCX N94

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Config Tool for MCX N94

4,829 Views
DmitryR
Contributor I

Hi all,

 

I am trying to start developing with MCX N94 MCU. I went to software and have found "MCUXpresso Config" there. I have downloaded and installed that but no matter what I try to do the tool says that the processor is not supported and I get only three nearly empty files (xxx.dtsi and pin_mux.x). No RTOS (I choose Zephyr), no HAL, nothing. If the processor is not supported then why is this tool resides in this processor's download area? And what tool do I need to use to configure MCX N94?

 

With best regards,

Dmitry

Labels (1)
0 Kudos
Reply
7 Replies

4,798 Views
DmitryR
Contributor I

Dear @Alice_Yang ,

 

please find attached.

 

Regards,

Dmitry

0 Kudos
Reply

4,735 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @DmitryR 

The Config tool supports MCXN947.
Please click the Pins tool icon.
 
pins.jpg

 

Also, please make sure you are using the latest version, V25.12.
I have recorded a video showing all the steps—please refer to the attachment.
 
Thank you.
 
BR
Alice

 

0 Kudos
Reply

4,726 Views
DmitryR
Contributor I

Dear @Alice_Yang ,

 

it's a pity but you did not understand right what I have written. I need not only the pin configuation, I need everything been generated: HAL, RTOS, and device configuration. What is the sense of choosing "Zephyr configuration" if it does not really generate Zephyr? Starting with bare pin_mux is very ineffective way of designing so I will not follow it. If it is not supported I am going to choose another microcontroller. If it will be supported in the nearest future please let me know.

 

Then, even pin muxing does not work completely. Your example works, but the configuration of USDHC does not. Please see the attached image.

 

Regards,

Dmitry

0 Kudos
Reply

4,720 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @DmitryR 

Thanks for your reply. I'm sorry, but currently the Config Tool only supports pin configuration based on Zephyr. I will check with the development team to confirm whether other device configuration features will be supported in the future. And send to you with any update.

For the error you provided, please review the error message.
 
Thank you.
 
BR
Alice
0 Kudos
Reply

4,717 Views
DmitryR
Contributor I

Dear @Alice_Yang 

 

what in this context then means "based on Zephyr" when Zephyr is also not generated? What at all sense is in this type of configuration?

 

Regards,

Dmitry

0 Kudos
Reply

4,466 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @DmitryR 

Thanks for your reply.
The tool support for Zephyr is still in an ongoing improvement stage, and more features will continue to be added over time.
Thank you.
 
BR
Alice
0 Kudos
Reply

4,797 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @DmitryR 

Thanks for your question. Which IDE are you using?
Or are you using the standalone MCUXpresso Config Tool?

Please take a screenshot or a short video showing all your steps, and I will help you check and confirm.


Thank you.

BR

Alice

 

 

0 Kudos
Reply