Hello NXP Support Team,
Board: FRDM-MCXE31B
I have a few questions regarding the debug-state configuration bits described in Table 574 of the MCXE31 Reference Manual.
1. Location and programming method of debug-state configuration bits
Table 574 describes the debug state for different combinations of the following configuration bits:
DBG_EN_OEM
APP_DIS_OEM
HSE_DIS_OEM
DBG_EN_FLD
APP_DIS_FLD
HSE_DIS_FLD
HSE_DIS_CUS
HSE_DIS_CR_MCU_PROD
HSE_DIS_PRE_FA
However, the Reference Manual does not clearly specify where these bits are physically located or how they are programmed.
Could you please provide the following information for each of these bits?
The memory/address location where the bit is stored.
Whether the bit is programmed through a UTEST DCF record.
The corresponding DCF record type/client and required record format.
The relevant DCF client documentation that describes how these bits are programmed.
Whether these bits can be programmed while the device is in CUST_DEL.
If they can be programmed in CUST_DEL, whether they can subsequently be modified or changed during the OEM_PROD or IN_FIELD stages.
If the bits are programmed as part of the LC transition, please clarify at which stage/LC state each bit is expected to be configured.
If there is a specific DCF Clients document, application note, or programming example for MCXE31 that describes this configuration, please provide the relevant document/reference.
2. OTP behavior and recovery
Are these bits OTP? If a wrong value is programmed, can the debug state be recovered?
This information is important for us to understand the correct provisioning sequence and to ensure that the debug configuration is programmed safely before advancing the device through the different Life Cycle states.
Thank you for your support.