AES-GCM performance on SE05x

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AES-GCM performance on SE05x

44 次查看
Viktro0929
Fresh Out Contributor

I am testing the capabilities of the SE050 on an OM-SE050X development board, and I have a question about the speed of the AES-GCM operation. It seems that when running a one-shot AES-GCM encryption with AAD, followed by decryption, the process takes around 8 to 9 seconds, even with small inputs in one-shot mode

I found a similar thread here discussing the same issue:

https://community.nxp.com/t5/Secure-Authentication/Re-SE050E-aead-encryption/m-p/1694085#M1317

The response there indicated that this is indeed expected, since the GCM part is not hardware-accelerated.

 

My questions are:

  • Can you please confirm whether this speed is normal, and whether there is any way to improve performance, or if software-based GCM will remain at this speed regardless?
  • Regarding the SE051 (or SE052), do these chips provide hardware acceleration for GCM, or any improvements in the speed of this operation?

 

Thank you in advance!

标签 (1)
0 项奖励
回复
1 回复

25 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Viktro0929 ,

 

Was it AES GCM 128 or 256? What about the data/AAD/IV length? From the test cases we have run, 8 to 9 seconds is little longer, what is the host controller you are using? Please kindly clarify.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复