Hi @martin_lapis
Thank you for your reply
Based on my understanding of this part, flash parameters can be adjusted through SPT. The modified parameters can be written to a specific block of the flash, and the ROM code will read the data from the flash. Then, it will configure the flash according to the settings defined by SPT, such as Max Frequency.
I’ve been using the same configuration version, so theoretically there shouldn’t be any differences. However, I’ve found that the flash on some devices is actually locked
That’s why I wanted to ask whether it’s possible that some mechanism in the ROM code operation might trigger the flash lock function(Non-Volatile Protection )