Pre-built image is loaded to the wrong location in FLASH

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pre-built image is loaded to the wrong location in FLASH

4,341件の閲覧回数
andrewmccartney
Contributor III

It appears that using the Secure Provisioning Tool to program a pre-built image into an RT1050 the image is placed at 0x60001000 instead of 0x60000000. This results in an image that does not boot. Using the SDP and BLHOST utilities from the command line and placing the same image at 0x60000000 the result is an image that boots correctly.

1. Why does the tool place the image offset by 0x1000?

2. Is there a way to change this offset?

Here is a snippet from the log file of the tool when it writes the image into FLASH.

/Applications/MCUX_Provi_v1/MCUXpresso Secure Provisioning Tools v1.app/Contents/MacOS/tools/blhost/mac/blhost -u 0x15A2,0x0073 -j -- write-memory 0x60001000 /Users/andrewm/MUN4_NXP_provisioning_tool/u-boot.bin 9

0 件の賞賛
返信
3 返答(返信)

4,247件の閲覧回数
andrewmccartney
Contributor III

Marek,

Thanks for the information, that's helpful in understanding how the tool works. Is there any way to change the settings of the tool in order to accommodate a bootable image that includes the FCB already?

thanks,

Andrew

0 件の賞賛
返信

4,247件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Andrew,

currently such image is not supported. However you can specify custom FCB content using:

toolbar - Boot Device - flex-spi-nor/user FCB file

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信

4,247件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Andrew,

write expects the bootable image without FCB configuration (_nopadding.bin). Typical workflow for images located in flash:

  • image (interrupt vector table) starts at 0x60002000
  • during build, bootable image is created with IVT (image vector table) starting at 0x60001000
  • during write, FCB (flash configuration block) is created at 0x60000000

You can find detailed description in the documentation, chapter Workflow.

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信