How to create OTFAD &HAB bootable images on Linux?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to create OTFAD &HAB bootable images on Linux?

Jump to solution
1,173 Views
Omar_hong
Contributor II

Hi NXP,

1. I know there are scripts files in this path for Linux(C:\Users\admin\secure_provisioning\build_image_lnx.sh), but I want to know if there are tools with features like "creat manufacturing package"? This is helpful for building image on different computers.

Omar_hong_0-1732183197214.png

2. When I press the 'Browse' button, SEC will automatically create the relevant files in this path(C:\Users\admin\secure_provisioning\source_images). How are these files created?

Omar_hong_1-1732183341672.png

Omar_hong_2-1732183439074.png

3 .This script uses nxpimage.exe. Can it run directly on Linux, or does it require Wine? Or is there a Linux version available?

Omar_hong_4-1732183780091.png

 

 

0 Kudos
Reply
1 Solution
906 Views
liborukropec
NXP Employee
NXP Employee

Hi,

 

could you install these packages as it is documented in the User Guide, chapter 4.4. Linux?

sudo apt install libhidapi-dev libsdl2-2.0-0

Regards,

Libor

View solution in original post

0 Kudos
Reply
16 Replies
1,153 Views
liborukropec
NXP Employee
NXP Employee

Hi Omar,

 

I'd add few notes:

ad 2) build (the same can be applied to write respectively) scripts are generated when clicking on "Build" button based on the workspace configuration.

ad 3) that no Wine is required, SEC tool provide support for Windows, Linux (Ubuntu) and MacOS (Intel+Arm). Based on the used OS the correct installer should be used and that's it. Only for Ubuntu - there are some dependencies, so SEC tool v 9.0.1 works in Ubuntu 22, while SEC v10 works on Ubuntu 24 (v10 Ubuntu 22 deb package will be released soon).

Regards,

Libor

0 Kudos
Reply
1,039 Views
Omar_hong
Contributor II

Hi @liborukropec 

ad 3) that no Wine is required, SEC tool provide support for Windows, Linux (Ubuntu) and MacOS (Intel+Arm). Based on the used OS the correct installer should be used and that's it. Only for Ubuntu - there are some dependencies, so SEC tool v 9.0.1 works in Ubuntu 22, while SEC v10 works on Ubuntu 24 (v10 Ubuntu 22 deb package will be released soon).

=> Does Linux version V9.0.1 support Ubuntu desktop or Ubuntu server, or both?"

0 Kudos
Reply
1,007 Views
liborukropec
NXP Employee
NXP Employee

Hello Omar,

>Does Linux version V9.0.1 support Ubuntu desktop or Ubuntu server, or both?"

it is intended for Ubuntu desktop, but I believe it could be installed also on Ubuntu server (without GUI) even it is not supported/tested. It will work only with CLI argument, like 'build', 'write'. Without CLI arguments it will try to launch GUI, where it will probably fail because of missing GTK dependencies and also noX/Wayland server.

Give it a try.

Regards,

Libor

0 Kudos
Reply
949 Views
Omar_hong
Contributor II

Hi @liborukropec ,

    I tried installing the following SPT Linux version on Ubuntu 22.04.5, but it still doesn't work. Could you please tell me what steps I might have missed?

It appears to have been successfully installed on the Ubuntu desktop 22.04.05 .When I click on SPT, there is no response from SPT.(No windows open or messages appear.)

Omar_hong_0-1732859630251.pngOmar_hong_1-1732859649134.pngOmar_hong_2-1732859667124.pngOmar_hong_3-1732859799675.png

 

 

0 Kudos
Reply
941 Views
liborukropec
NXP Employee
NXP Employee

Hi Omar,

have you used the deb package for ubuntu22?

liborukropec_0-1732870045505.png

 

Please open Terminal and execute

# if you notice UI glitches, uncomment the export command
# UBUNTU_MENUPROXY=0 GDK_BACKEND=x11 /opt/nxp/MCUX_Provi_v10/bin/securep
/opt/nxp/MCUX_Provi_v10/bin/securep

most probably in the output there will be clear what is the problem and you can paste it here.

 

Regards,

Libor

0 Kudos
Reply
932 Views
Omar_hong
Contributor II

Hi @liborukropec ,

  The result is as attached file.

 

  

0 Kudos
Reply
925 Views
liborukropec
NXP Employee
NXP Employee

HI,

you doubled the SEC path in the terminal, that's why it opened only help.

you should run either:

/opt/nxp/MCUX_Provi_v10/bin/securep

or:

UBUNTU_MENUPROXY=0 GDK_BACKEND=x11 /opt/nxp/MCUX_Provi_v10/bin/securep


Could you please try again?

Libor

0 Kudos
Reply
915 Views
Omar_hong
Contributor II

Hi @liborukropec 

  Thanks for your quick reply.

    The result is as attached file.

0 Kudos
Reply
907 Views
liborukropec
NXP Employee
NXP Employee

Hi,

 

could you install these packages as it is documented in the User Guide, chapter 4.4. Linux?

sudo apt install libhidapi-dev libsdl2-2.0-0

Regards,

Libor

0 Kudos
Reply
884 Views
Omar_hong
Contributor II

Hi @liborukropec 

  Thanks for your quick reply.

      It seems to be starting up normally now. Thank you very much. !

0 Kudos
Reply
1,158 Views
marek-trmac
NXP Employee
NXP Employee

Hi Omar,

ad 1) SEC tool does not support creation of manufacturing package on command-line. It is supported in GUI only.

ad 2) SEC tool parses the source image and convert to the format, that will be needed on the build. This feature is same for GUI and for the build CLI command.

d 3) Go to https://nxp.com/mcuxpresso/secure and download the SEC tool for Linux. It contains all tools compiled for Linux. Supported operating system version are described in release notes.

Regards,
Marek
0 Kudos
Reply
1,136 Views
Omar_hong
Contributor II

ad 2) SEC tool parses the source image and convert to the format, that will be needed on the build. This feature is same for GUI and for the build CLI command.

=>Could you please provide specific commands or methods to generate those files? (.serc .bin)

Omar_hong_0-1732210100760.png

 

0 Kudos
Reply
1,130 Views
marek-trmac
NXP Employee
NXP Employee

Hi Omar,

see command nxpimage utils binary-image convert.

For description, please refer to SEC tool command: main menu > Help > SPSDK Online Documentation.

Regards,
Marek
0 Kudos
Reply
1,147 Views
marek-trmac
NXP Employee
NXP Employee

Hi Omar,

for the first question, do you have any reason to create manufacturing package on CLI? We understand it is good to have a build available for continuous integration, but for the manufacturing package - this is created once you are ready to send the code to FAB. I do not see any reason to automate that. Why did you ask for CLI version?

Regards,
Marek
0 Kudos
Reply
1,140 Views
Omar_hong
Contributor II

Hi @marek-trmac 

I think you misunderstood my mean. What I want is a feature that can package the tools needed to build the boot image into a zip file.(It can be executed on the Windows version of SEC)

0 Kudos
Reply
1,134 Views
marek-trmac
NXP Employee
NXP Employee

Hi Omar,

the only distribution of the executable tools is available on NXP.com https://nxp.com/mcuxpresso/secure via the MCUXpresso installers. Currently there are no plans for other distribution.

Regards,
Marek
0 Kudos
Reply