i.MX RT1060 SDK 2.15 Support for 88W8987 WiFi RTT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT1060 SDK 2.15 Support for 88W8987 WiFi RTT

1,296 Views
jfs17
Contributor II

Hi,

Our team currently are starting to explore indoor positioning system, particularly on IEEE 802.11 mc and I am looking for a Wi-Fi device to work on. I checked that 88W8987 as per datasheet says that supports "Wi-Fi indoor location positioning (802.11mc)".

I also found that I can use i.MX RT1060 as host MCU connected to 88W8987 module. However when I checked the SDK version 2.15, I did not find any API or process to trigger RTT/FTM request and respon

Can you guys tell me if I missed something on the SDK or confirm that I can use i.MX RT1060 and 88W8987 to perform WiFi RTT indoor positioning?

Thanks.

Tags (3)
0 Kudos
Reply
1 Reply

1,281 Views
cdoumenc
NXP Employee
NXP Employee

Hi,
Let me check internally

0 Kudos
Reply