When or will the flexio RGB lcd interface driver release out ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When or will the flexio RGB lcd interface driver release out ?

2,415 Views
rqbh
Contributor III

As the title , will the flexio driver support lcd RGB interface ?

I'm using the mk27 mcu.

0 Kudos
Reply
2 Replies

2,226 Views
carlos_chavez
NXP Employee
NXP Employee

Hello rqbh‌,

Just for your information in case you were not aware, we have the following App Note that implements an RGB FlexIO Driver for the K80 device.  The FlexIO used on the K27 and K28 devices are the same IP as used on the K80. 

https://www.nxp.com/docs/en/application-note/AN5280.pdf 

The 8080 interface found in the MCUXpresso SDK used the driver referenced in AN5280 as a starting point.

BR,

Carlos

0 Kudos
Reply

2,226 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi kevin shang 

SDK supports flexio 8080 interface, but not RGB interface. Currrently no plan for RGB interface.

There is a FlexIO LCD demo for K28, and K27 is K28f project subset

boards/frdm28f/demo_apps/flexio_mcu_lcd

Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply