Unable to download SDK for MK10DX64VLH7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to download SDK for MK10DX64VLH7

1,916件の閲覧回数
mylim
Contributor IV

Hi, I am using MCUXpresso IDE. I would like to find out how to get SDK for MK10DX64VLH7. 

When access the SDK dashboard I am only able to find the list of SDK below.

Please help.

pastedImage_1.png

ラベル(1)
タグ(2)
7 返答(返信)

1,773件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi mylin,

MCUXpresso doesn't support MK10DX64VLH7. Please use KDS, Codewarrior or other IDE. The attachment is the example and driver package.

Regards,

Jing 

0 件の賞賛
返信

1,773件の閲覧回数
mylim
Contributor IV

Hi, thanks for the reply. I tried KDS 3.2. However, when i create new project using kinetis SDK 2.X project wizard i couldn't download the kinetis SDK for MK10DX64VLH7.

I understand there have been some change in platform from KDS to MCUXpresso. If there any link i can download the legacy files? 

Thanks.

0 件の賞賛
返信

1,773件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

no, there isn't SDK for 72MHz MK10. Only 100MHz product in MK10 family has SDK. You can start from Processor Expert in KDS.

Regards,

Jing

0 件の賞賛
返信

1,773件の閲覧回数
mylim
Contributor IV

Hi, Thanks. I would like to find out is there any RTOS support for MK10DX64VLH7? 
otherwise, which would be the 64pin or less pin count has RTOS support?

Please advise.

Thanks.

MY

0 件の賞賛
返信

1,773件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

MQX4.2 has TWR-K20D72M in its supporting list. TWR-K20D72M support K10D72M. So, you can use MQX4.2 directly.

Regards,

Jing 

0 件の賞賛
返信

1,773件の閲覧回数
mylim
Contributor IV

Hi Jing,

 I found out that 'MQX v4.2 is no longer available & superseded by v5.' 
In that case the latest 5.1 supports? or is there anywhere i can get my hands on v4.2? 

Thanks.

0 件の賞賛
返信

1,773件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Yes, you're right. MQX v4.2 is no longer avaiable on NXP portal. V5.1 is not for free and I have no idea about it. Maybe you can refer to this link for v4.2. Freescale MQX RTOS 4.2.0-MQX实时操作系统-恩智浦技术社区 

If you have any questions about the legacy MQX 4.x, you can create a ticket to NXP technical support.

Support | NXP 

Regards,

Jing

0 件の賞賛
返信