USB CDC Serial Port

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB CDC Serial Port

2,746件の閲覧回数
DG_PIPE
Contributor I

Hello,

I am currently making a project with the MXUXPRESSO SDK , on an NXP microcontroller.

(MCUXpresso IDE , MKL27z256xxx4 MCU. to be specific)

I've been able to get the USB CDC Serial Port configured in the peripherals perspective , however I can't find any libraries or code to interface with to give me access to the USB CDC Serial port , only low level usb transaction level access.

I would have assumed that a usb serial port isn't something that is so bespoke that it would be re-written every time , and that I just don't know where to look.

If it is something that would need to be written bespoke , any guidance would be appreciated

Any help pointing me in the correct direction would be appreciated.

Daniel

 

 

0 件の賞賛
返信
2 返答(返信)

2,736件の閲覧回数
DG_PIPE
Contributor I

Hi VaneB,

Your Quick Reply and guidance is much appreciated , I'll have a look into that

Daniel

0 件の賞賛
返信

2,742件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @DG_PIPE 

Please enter to the following link: SDK and download the last SDK version of the FRDM-KL43Z, there you can find the drivers and also some examples for USB.

 

B.R.

VaneB

0 件の賞賛
返信