Hi,
I followed the installation instructions from, FRDM-KW41Z|Freedom Development Kit|NXP , which was linked to in my quick start guide. however, the wireless example demo codes do not run properly as expected.
When building the ble_thread_router_wireless_uart example project, I get a compilation error, in ble_controller_task.c and app_config.c saying that 2 variables are declared not inside a function.
I haven't even edited the code, so I'm not sure why there is a syntax error.
Can I check if anyone knows what is the problem?
Hi Lau,
I compiled the ble_thread_router_wireless_uart project. I didn't find any problem. So maybe you can try to download the SDK package again and recompile it.
Regards
Hi Jing Pan,
Thanks for the reply. I have tried re-downloading the SDK from the link provided at FRDM-KW41Z|Freedom Development Kit|NXP , but the same thing still happens.
A similar build error happens when I run any other of the wireless_examples, but the driver_examples and the demo_apps run fine.
I also realized that I could not find a main function in any of my wireless examples. I think that was probably what caused the build error.
Do you have any idea what might have caused this?
Thanks!
Hi guys,
I figured out the problem. For whatever reason, the sdk provided at FRDM-KW41Z|Freedom Development Kit|NXP  did not work for me. I had to go to Welcome to MCUXpresso | MCUXpresso Config Tools  and use the SDK builder provided there. That eventually worked.
I hope this helps anyone with similar problems.