Redirect SHELL GETCHAR to custom implementation missing?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Redirect SHELL GETCHAR to custom implementation missing?

1,975件の閲覧回数
robertoquilez
Contributor III

In the previous version, a nice feature that now is missing was to redirect the GETCHAR (SHELLReveiveDataCallBack) to a custom implementation. For instance, this enabled to implement a GETCHAR version with a SHELL freertos task in SUSPENDED STATE while waiting for a character. 

Is there a way to redirect the GETCHAR to a custom application as before with the new SDK shell version?

By the way, the SHELL in SDK 2.5.0 documentation (MCUXpresso SDK API Reference Manual_MK66F18.pdf) does not match the source code.

Documentation refers to : 

SHELL_Init(&user_context, SHELL_SendDataCallback, SHELL_ReceiveDataCallback, "SHELL>> ");

When the SDK source code:

    shell_status_t SHELL_Init(shell_handle_t shellHandle, serial_handle_t serialHandle, char *prompt);

0 件の賞賛
返信
2 返答(返信)

1,816件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Roberto Quilez

The implementation in the SDK 2.4 version uses callbacks for the "send" and the "receive" functions. Now in SDK 2.5, those parts are managed in the serial_manager component, so if you want to change this, you can do it in the SerialManager_StartReading function in the serial_manager.c/.h

Regarding the documentation, thanks for pointing out this, I will report this for future releases.

Hope this information helps
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,816件の閲覧回数
robertoquilez
Contributor III

Thank you very much, Joge,  for your rapid response.

From my personal use case and personal point of view,  I think that it is a pity to have to modify the source code of one of the SDK components.  Every time I update the SDK, I might loose my modifications and I will have to take care of including them manually.

I think the previous implementation was more convenient as it was part of the shell initialization settings.  Actually I have the impression that it is much more complex (and limited) that the previous one.

0 件の賞賛
返信