Re: FLEXIO_CAMERA_Init

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: FLEXIO_CAMERA_Init

1,671 Views
danielchen
NXP TechSupport
NXP TechSupport

HI Wenda:

Which MCU you are using?

Regards

Daniel

0 Kudos
Reply
2 Replies

1,549 Views
1104883515
Contributor I

RT1052, can you tell me where I can get these libs(fsl_flexio_camera, fsl_flexio_camera_adapter,fsl_flexio_camera_edma  )

0 Kudos
Reply

1,549 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Wenda:

The flexio interface is for Kinetis parts. Not sure this example has ported to i.mx RT .

The i.MX RT1050 processor has the special camera sensor interface (CSI) module, especially meant for parallel camera connection. So, there is no need of using FlexIO modules.

For the example of the CSI module use, please refer to the AN12110 Application note and the corresponding example, available on below link

https://www.nxp.com/docs/en/application-note/AN12110.pdf 

pastedImage_2.png

Regards

Daniel

0 Kudos
Reply