RT1064 lwip_httpssrv_mbedTLS_freertos

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1064 lwip_httpssrv_mbedTLS_freertos

1,037件の閲覧回数
newtofourms
Contributor I

Hello,

 

So started to mess around with mbedTLS on the RT1064-EVK and the lwip_httpssrv_mbedTLS_freertos example implementation doesn't seem to work. I get a site can't be reached error but the SSL certificate is being served. If you were to disable mbedTLS in the pre-processor config and try to access over http, it works. Additionally the lwip_httpssrv_mbedTLS_bm example works too. Any ideas what could be wrong??

Attached below is the project file.

 

 

0 件の賞賛
返信
1 返信

1,023件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

This is an issue for FreeRTOS MCUXpresso debug target. It will be fixed in next release.  It works for the release target. 

Also works for IAR or Keil.

 

 

Regards

Daniel

 

0 件の賞賛
返信