LA_OPT_NXP_Software_License RTAudio January 2019

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LA_OPT_NXP_Software_License RTAudio January 2019

2,189 Views
shingofujiwara
Contributor II

In section 2.2 and 2.5, 

for example, when we develop software with outsource, we can not share SDK ?

"outsource" means software development company in other city or nation.

Or, can I share to outsource some source code with BSD-3-Clause.

for example, can I share part of SDK package "SDK_Peripheral_Driver " to outsource.

SDK_Peripheral_Driver Name: SDK Peripheral Driver
Version: 2.x.x
Outgoing License: BSD-3-Clause
License File: COPYING-BSD-3
Format: source code
Description: Peripheral drivers are designed for
the most common use cases identified for the
underlying hardware block.
Location: devices/<device>/drivers
Origin: NXP (BSD-3-Clause)

 

0 Kudos
Reply
1 Reply

2,172 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Please help me to contact your local NXP representative to check if there is any legal issue with this 

regards

 

0 Kudos
Reply