I2C DMA driver problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2C DMA driver problem

2,233件の閲覧回数
microcris
Contributor III

Hello!

I made a FreeRTOS I2C DMA implementation (based on the SDK i2c DMA driver example) and it is running fine. But...

...But I found a problem that I think is worth being reviewed.

While sending data (in my case:  start + 1 slave address byte+ 1subaddress byte  + 1 data byte), "I2C_RunDMATransfer" function is called more than one time and almost simultaneously  "I2C_RunTransferStateMachineDMA" is also called by the IRQ ("I2C_MasterTransferDMAHandleIRQ"). It happens that both functions can change the "remainingBytesDMA" variable. So, when "I2C_RunDMATransfer" is called, the "remainingBytesDMA" is 1 and before "I2C_RunDMATransfer" ends the "remainingBytesDMA" variable is changed to 0, then in the end of "I2C_RunDMATransfer" that operation "handle->remainingBytesDMA -= transfer_size;" is made and the "remainingBytesDMA" goes from 0 to a very big number and later "DMA_PrepareTransfer" asserts in "(xfer_count <= DMA_MAX_TRANSFER_COUNT) && (0 == transferBytes % byteWidth)"

As a workaround I made the following change in "I2C_RunDMATransfer":

changed this
DMA_SubmitTransfer(handle->dmaHandle, &xferConfig);
DMA_StartTransfer(handle->dmaHandle);
handle->remainingBytesDMA -= transfer_size;
handle->buf += transfer_size;    


to that
DMA_SubmitTransfer(handle->dmaHandle, &xferConfig);
DMA_StartTransfer(handle->dmaHandle);
if(handle->remainingBytesDMA >= transfer_size)
{
        handle->remainingBytesDMA -= transfer_size;
}
else
{
        handle->remainingBytesDMA = 0;
}
handle->buf += transfer_size;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

In the attached file I have the FreeRTOS inplementation, if you need it.

 

タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,049件の閲覧回数
microcris
Contributor III

Hello Daniel,

Here it is:

LPC54628J512

SDK2.5.0

I2C DMA driver version 2.0.3

0 件の賞賛
返信

2,049件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

HI  Cristiano:

Thank you very much for your feedback, could you please let me know the MCU you used and the SDK version?

Regards

Daniel

0 件の賞賛
返信