Flexbus example fails

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flexbus example fails

2,138 次查看
yorknh
Contributor IV

I've downloaded an MCUXpresso 2.2 SDK for the TWR-K64F120M. I imported the flexbus driver example and successfully compiled and loaded the code. When I run the code, it prints out: 

FLEXBUS Example.

Initialize FLEXBUS.

Start write/read MRAM.

FLEXBUS (MRAM) test: failed.

I haven't modified any code, so I would expect it to succeed. Has anyone else had this work?

I have the flexbus working correctly on the same board using the KDS3.0 and KSDK1.3.0. I was trying to port this working code to the new MCUXpresso environment and was having issues, so I figured I would build the example to use as a reference. Since the example doesn't work, it doesn't serve as a useful reference.

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,936 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Larry:

I did a quick check about this demo, it works on my side. I would suggest you check the jumper settings in your TWR-MEM board.

pastedImage_1.png

Regards

Daniel

0 项奖励
回复