Compatible SDK for LPCXpresso4367

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compatible SDK for LPCXpresso4367

1,379件の閲覧回数
mario_goeckel_e
Contributor I

hi folks,

i use a LPCXpresso4367-board with ARM-M4.

when searching at MCUXpresso SDK using board/processor/kit as input for the SDK-builder, not SDK could be found. is there maybe another SDK, which is compatible to the LPCXpresso4367-board i use?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,217件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

 

Unfortunately, there is no SDK for LPC43xx family devices. We currently have no plans to provide MCUXpresso SDK for this device family.

You can use the LPCOpen Software for LPC43xx devices, LPCOpen is an extensive collection of free software libraries (drivers and middleware) and example programs that enable developers to create multifunctional products based on LPC microcontrollers. Access to LPCOpen is free to all LPC developers.

Please check the below link:

http://www.nxp.com/products/software-and-tools/software-development-tools/software-tools/lpcopen-lib...

 

In addition, please check the below document, this explains how to create a new LPC project using LPCOpen and MCUXpresso IDE.

How to create a new LPC project using LPCOpen and MCUXpresso IDE 

 

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信