Basic timer usage for periodic operation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Basic timer usage for periodic operation

1,466件の閲覧回数
next_devenv
Contributor I

Hi,

Could the community pls advise guidance, some refs or example/sample code for a basic use of a precision timing operation, for a newbie?

I'm using the QN908x DK, and would like to perform a specific operation every 10u seconds.

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

1,402件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

It will depend on which kind of operation you need. Is the operation with the usage of the Wireless Connectivity Stack or is it just to get to know the MCU within it's peripherals?

I would recommend you to start with some of the driver and demo examples available in the SDK that you can download from this page as well as you can download the IDE.

If you want to understand in a general view Bluetooth LE and a little bit of the stack you can check this video series, those videos are for the KW41 the stack is very similar to the QN9080.

Regards,

Estephania

0 件の賞賛
返信