v11.5.0 unstable debugger om Ubuntu

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

v11.5.0 unstable debugger om Ubuntu

2,413件の閲覧回数
erling
Contributor III

I am using iMXRT1170 EVK with MCU Link Pro as the debugger. The new version of MCUXpresso was even more unreliable than v11.4.1. More or less 50% of the times I start a debug session it fails and I must power cycle both EVK and MCU Link Pro. I am using Ubuntu 18.04:

erling@ubuntu-ntnu ~> uname -a
Linux ubuntu-ntnu 5.4.0-99-generic #112~18.04.1-Ubuntu SMP Thu Feb 3 14:09:57 UTC 2022 x86_64 x86_64 x86_64 GNU/Linux

0 件の賞賛
返信
4 返答(返信)

2,312件の閲覧回数
erling
Contributor III
 
0 件の賞賛
返信

2,312件の閲覧回数
erling
Contributor III

Problem is both with on-board debugger and MCU Link Pro. Here is the save-log

0 件の賞賛
返信

2,370件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Hi,

We cannot reproduce locally this problem. It is possible to pack the eclipse log plus console logs and send us to investigate? You can achieve this by using Save Info for Support option which generates a zip file with all the logs:

lpcxpresso_supp_0-1645608752668.png

When choosing this option, all files going to archive will be listed. We recommend to let them all selected as they are set by default.

Regards,

MCUXpresso IDE Support

0 件の賞賛
返信

2,388件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
When using the on-board debug tool instead of MCU Link Pro, does the unstable debugging phenomenon also happen?
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信