project disappears from the MCUXpresso IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

project disappears from the MCUXpresso IDE

1,646 Views
zili_zhang
Contributor I

Hi,

I have a project set up in MCUXpresso IDE on a VM with Ubuntu Linux. I built the code fine in the IDE. But sometimes after I power off the VM and power it back on, the project disappears from the IDE. I googled it but did not see any post for the same issue. Does anyone have any ideas about the issue?

Thanks

0 Kudos
Reply
3 Replies

1,532 Views
zili_zhang
Contributor I

Hi Daniel,

Thank you for your reply.

Yes it can be reproduced. I just tried it yesterday. Set up a project in the IDE (VERSION 11.1.1) and compiled and built the SW all fine. But after powering off the VM and powering back on, the project disappeared from the IDE. I tried going through the same process more 2 times and got the same results - project disappeared from the IDE.

Thanks again,

Zili Zhang

0 Kudos
Reply

1,532 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi zili:

It seems workspace not saved in your case. I would suggest you exit workbench before you powering off the VM.

pastedImage_1.png

Regards

Daniel

0 Kudos
Reply

1,532 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Zili:

Can you reproduce this issue?

Regards

Daniel

0 Kudos
Reply