Hi
using SDK example "flexSPI_nor_polling_transfer"
I need to set more commands on the LUT.
the costume LUT size is 60 and if the step is 4 between each command, I can only use 15 commands.
I need to use more to support this FLASH device : W25Q128FV pdf, W25Q128FV Description, W25Q128FV Datasheet, W25Q128FV view ::: ALLDATASHEET :::
but if I set the table size to 80, any value after 60 is ignored\not working even after I change the define:
#define CUSTOM_LUT_LENGTH 60
any help?
Adi
Intel
已解决! 转到解答。