Wire ACK Fault in DAP Access: Debugger won't run

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wire ACK Fault in DAP Access: Debugger won't run

1,977件の閲覧回数
jordiclos
Contributor I

I am trying to debug with MCUxpresso IDE v10.1 a gpio example (gpio_led_output) and when I try to debug it appears that error.

I also tryied to erase flash memory and reinstall the mbed driver for windows but the error still appearing.

Someone know how to solve it and debug correctly?

Thanksdebug problem.JPG

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,748件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

What OS / version are you running on?

Have you been able to successfully debug this board previously?

Can you also confirm which board you are using? [I presume from the example you are trying to debug that it is a TWR-KV11Z75M, but it would be good to confirm.] It might also be worth ensuring that the OpenSDA has the latest firmware in it (from http://www.nxp.com/opensda), or even trying the alternate firmware images for SEGGER / P&E rather than the mbed/CMSIS-DAP.

Regards,

MCUXpresso IDE Support