What is the "Run" icon in the toolbar for?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the "Run" icon in the toolbar for?

1,220 次查看
submod
Contributor I

Hello,

What is the Run Icon in the toolbar (at the top of the application next to the debug ones)? Everytime I click it it seems to do nothing except start a debug session which there is no way of stopping without closing MCUxpresso and restarting? It always gives the error "There is already a running debug session......"

I was expecting it to just uplaod code and run (with out breakpoints) but that doesnt seem the case.

I'm using the LPC1769Xpresso boards....

Thanks

0 项奖励
回复
1 回复

1,130 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Matthew Todman ,

About download code and debug, please use "Debug..." under "Quickstart Panel":

pastedImage_2.png

or the icon of below :

pastedImage_1.png

About run please use this icon:

pastedImage_3.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复