Warning from MCUXpresso IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Warning from MCUXpresso IDE

1,667 Views
jamesli
Contributor IV

Dear,  

 

Here is warning from IDE and it seems does not prevent me to run the code. How to fix the problem!

jamesli_0-1761752195577.png

Thank you in advance!

Jian Li

 

0 Kudos
Reply
2 Replies

1,629 Views
ErichStyger
Specialist I

What IDE version and more specific which gdb are you using?

The thing is that this message comes from a bug of gdb: in most cases you can simply ignore it. I had it too, and usually it has no impact.

But if in case you are not able to debug that file, what helped me is to create a new file with a text editor, and copy the file content into it.

I hope this helps,

Erich

0 Kudos
Reply

1,637 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @jamesli 

Please try making a new workspace before creating/importing the project that you are using. As mentioned on the following post, it's always a good idea to create a new workspace when changing IDE version:

MCUXpresso + Jlink - Cannot convert encoding - NXP Community

BR,
Edwin.

0 Kudos
Reply