Upload and run example projects on LCP1549

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Upload and run example projects on LCP1549

9,491件の閲覧回数
stevemeister
Contributor I

Hi!   I installed MCUXpresso IDE v10.1.1 on my MacBook Pro (macOS High Sierra): I tried to build then debug the example project "periph_blinky" on OM13056: LPCXpresso™ Board for LPC1549. After probe recognition the debugging session never ends.

At the bottom left of the window it says me “Connect to target”, the project is not loaded on the board and the led doesn’t blink. The keys "Resume","Suspend"and"Terminate" keys are never available in the toolbar. Thank you.

0 件の賞賛
返信
3 返答(返信)

9,350件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

What board / debug probe are you using? Is this an LPCXpresso1549 board, and using CMSIS-DAP firmware?

Can you provide the details from the debug log and also the redlinkserver log in the console view, as described in section 16.8, "The Console View" of the MCUXpresso IDE v10.1 User Guide .

Regards,

MCUXpresso IDE Support

0 件の賞賛
返信

9,350件の閲覧回数
stevemeister
Contributor I

I added new screen shots

0 件の賞賛
返信

9,350件の閲覧回数
converse
Senior Contributor V

Towards the end of the console log, there is a message that say 'localhost- no such host'. That implies there is a problem with your network configuration. Every system shound have localhost set up. So I suggest that is where you start.

0 件の賞賛
返信