The version of IDE can support S12G64 for CWS12v5.2 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The version of IDE can support S12G64 for CWS12v5.2 ?

1,091 次查看
yanlaidong
Contributor I

I do not find the S12G64 of mcu ,for the CWS12v5.2. 

0 项奖励
回复
1 回复

1,021 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Yes, the CW5.2 delete some devices.

While it doesn't matter,

Please refer to the below thread add missing device :

https://community.nxp.com/message/908307

Or you can use CW5.1 .

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复