Starting debugger using MCUXpresso fails under Debian

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Starting debugger using MCUXpresso fails under Debian

513件の閲覧回数
achampoux
Contributor I

IDE: MCUXpresso v11.8.0

SDK: SDK_2_14_0_MIMXRT1170-EVKB-LINUX

Target board: MIMXRT1170-EVKB

Trying debug an m7 project fails with the message: 'Launching m7 LinkServer Debug' has encountered a problem, problem file does not exist. The file path to the binary is "m7/Debug\m7.axf", which contains an error as it contains a "\" instead of "/". The build is successful, the board is detected and the file does "m7/debug/m7.axf" exists.

Any way to fix this? 

Thanks.

0 件の賞賛
返信
1 返信

458件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @achampoux 

How about first debug a SDK demo without any change?

 

BR

Alice

0 件の賞賛
返信