Question about Hexiwear

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about Hexiwear

1,773 Views
fabig
Contributor I

Hi,

I'm trying to use the example projects provided by Hexiwear on their github.

I'm using MCUxpresso 10.2.0 with the Hexiwear SDK. The example projects from the SDK work, the whole project from the Hexiwear Github doesn't work. It's giving me a "Program "-E" not found in PATH" error, so I cannot build it. What is required to fix this?

Best regards

Labels (1)
0 Kudos
Reply
1 Reply

1,584 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Fabi G,

   Do you mean the HEXIWEAR code download from this link?

GitHub - MikroElektronika/HEXIWEAR: HEXIWEAR firmware 

  The project on this package is using KDS IDE, not the MCUXpresso IDE, so if you use the MCUXpresso IDE, it will have problems.

  Please refer to the HEXIWEAR - Getting started.pdf in folder : HEXIWEAR-master\HEXIWEAR-master\documentation

  You will find the project is based on KDS.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------