Not able to Flash the LED blinking example code in FRDMK-64 F development board using MCUXpresso IDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Not able to Flash the LED blinking example code in FRDMK-64 F development board using MCUXpresso IDE

2,412 次查看
Megha
Contributor II

Hi,

I imported Blinky_LED code from example projects in MCU X presso IDE and compiled without error and loading in to Frdmk-64F development board, it is not loading showing the not able to detect target and some time error from debugger end:

connections are line : 1 USB cable connected from J26.

Debugger settings in tool : J link interface USB : 123456

                                           Device : MK64FN1M0xxx12

                                            Target Interface : SWD

                                            Speed : Fixed and 1000Khz

please suggest me if any problems in hardware jumpers and any settings changes are needed in the tool?

 

 

0 项奖励
回复
2 回复数

2,399 次查看
PabloAvalos
NXP TechSupport
NXP TechSupport

Hi, @Megha 

 

Thank you so much for reaching us and thank for all your patience.

 

When you go to the debug session (load the program to the flash), do you see a screen like this? 

PabloAvalos_0-1641567228932.png

If not, may you share with me the error that is appearing you? So I can help you.

Also, please take in consideration that you have to have installed the Segger J-Link driver and your USB connected in J26 is for transmit-receive data.

 

Please let me know if the problem persist, you I can help you further.

 

Best Regards.
Happy NY.
Pablo Avalos.

 

0 项奖励
回复

2,382 次查看
Megha
Contributor II

Hi,

Thanks for the reply.

The issue is solved and it is working fine, the issue is one of the jumper we missed on the Eval board.

0 项奖励
回复