Missing peripherals tools in MCUXpresso IDEv11.6.0 in project with SDK_2_11_0_MKE06Z128xxx4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Missing peripherals tools in MCUXpresso IDEv11.6.0 in project with SDK_2_11_0_MKE06Z128xxx4

跳至解决方案
916 次查看
CMH1
Contributor II

Hello All,
Using MCUxpresso 11.6.0 and SDK MKE06Z128xxx4 Version 2.11.0 for processor MKE06Z128VLD4. Not sure if it's something I've done but several peripherals are missing from the peripherals tool. The drivers are available when setting up a new project, source and header files are created in the project. For example, MSCAN/Flexcan, ADC, RTC are not show. See the attached screen shots showing the peripheral config page and the Manage SDK window. Any ideas?

0 项奖励
回复
1 解答
906 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi CMH1 

For the moment  MSCAN/Flexcan, ADC, RTC are not implemented in peripheral tool in KE128. I will escalate it as feature request to config tool team.  Please use SDK component for these peripheral.

Thanks for bringing the problem to our attention.

Have a nice day,

Jun Zhang

在原帖中查看解决方案

0 项奖励
回复
2 回复数
902 次查看
CMH1
Contributor II

Thank you for the help. 

0 项奖励
回复
907 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi CMH1 

For the moment  MSCAN/Flexcan, ADC, RTC are not implemented in peripheral tool in KE128. I will escalate it as feature request to config tool team.  Please use SDK component for these peripheral.

Thanks for bringing the problem to our attention.

Have a nice day,

Jun Zhang

0 项奖励
回复