Hello All,
Using MCUxpresso 11.6.0 and SDK MKE06Z128xxx4 Version 2.11.0 for processor MKE06Z128VLD4. Not sure if it's something I've done but several peripherals are missing from the peripherals tool. The drivers are available when setting up a new project, source and header files are created in the project. For example, MSCAN/Flexcan, ADC, RTC are not show. See the attached screen shots showing the peripheral config page and the Manage SDK window. Any ideas?
解決済! 解決策の投稿を見る。
Hi CMH1
For the moment MSCAN/Flexcan, ADC, RTC are not implemented in peripheral tool in KE128. I will escalate it as feature request to config tool team. Please use SDK component for these peripheral.
Thanks for bringing the problem to our attention.
Have a nice day,
Jun Zhang
Thank you for the help.
Hi CMH1
For the moment MSCAN/Flexcan, ADC, RTC are not implemented in peripheral tool in KE128. I will escalate it as feature request to config tool team. Please use SDK component for these peripheral.
Thanks for bringing the problem to our attention.
Have a nice day,
Jun Zhang