Memory view

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Memory view

3,314件の閲覧回数
carstenhoffmann
Contributor I

Hi,

I am using MCUXpresso and I have a beginners question.

Everytime I start a new debug session (with terminate, build, debug), all my memory monitors are removed.

I have to add them by hand for each new session.

Is there any way to keep the memory monitors?

Thanks for help,

Carsten

0 件の賞賛
返信
1 返信

3,083件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Sorry, no. There is no way currently of automatically re-populating the Memory View from previous debug sessions.

Couple of things that may help to a degree. If you are viewing memory at the base addresses of RAM or Flash regions defined for the project, then these will be listed for quick selection towards the bottom of the list of peripherals in the Peripherals View. In addition the + button in the Memory View will keep a list of previously viewed memory locations in the drop down for the duration of the IDE current session, which can save having to type the address in again.

Regards,

MCUXpresso IDE Support

0 件の賞賛
返信