MCUxpresso GUI Flash Tool program KW38 over Flas size 0x40000 issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUxpresso GUI Flash Tool program KW38 over Flas size 0x40000 issue

1,464件の閲覧回数
Kris_Ke2048
Contributor I

Dear 

I want to use GUI Flash Tool of MCUXpresso to programming attach file, but I find it can't work.

 

But if I use IAR to programming attached file, it seems it will be programming successful. 

For example, I use FRDM-KW38 EVB with IAR to programming, the UART console will show 

console.png

 

The LED4 will be twinkle white, when I press SW3, LED4 turns to flashing red.

Then I check the Flash memory address, the Flash address 0x40000 will have data.

擷取.PNG

 

 

Then I use GUI Flash Tool of MCUXpresso(v11.5.0 [Build 7232] [2022-01-11])  to programming same file, it will show "Unable to perform operation!  Command failed with exit code 1)

 

programming_1.pngprogramming_2.png

 

 

Then I unplugged the USB, plugged it back in, and found that LED1 is always on red, I looked at the wiring schematic and confirmed that this should be the Reset pin that is always grounded.

Kris_Ke2048_2-1656671664237.png

 

 

Then I set Attach only and Reset on Connect in Debug Configurations to check memory.

Then I found that only burned to 0x3FFFF, more than 0x40000 are not properly program.

Kris_Ke2048_0-1656671351620.png

 

This is the binary file attached.
Anything over 0x40000 has not been properly burned by the GUI Flash tool.

Kris_Ke2048_1-1656671500385.png

 

Is it impossible to show more than 0x40000 content that is burned by MCUXpresso?

 

Thanks,

Kris

タグ(2)
2 返答(返信)

1,414件の閲覧回数
Kris_Ke2048
Contributor I

Dear Eduardo

I've try use J-Link with MCUXpresso 11.5  can be successfully burned.

And the SDK version is SDK_2_6_212_FRDM-KW38.

 

Kris

0 件の賞賛
返信

1,431件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

I apologize for my late response.

Could you please help me with more details about which version of the SDK are you using?

Would it be possible to test the Flash Tool by using a binary file from another example project? Just to confirm this behavior.

The size of the binary file that you attached caught my attention. Is your project based on the shell example from the SDK? Could you please help me with more details about what modifications you made to the base source code?

Regards,
Eduardo.

0 件の賞賛
返信